WindowPos

Arguments

10 integers, e.g., " 0,1,-1,-1,-1,-1,390,107,1103,643"

Special

This entry is only considered at startup. Later load operations do not use it afterwards.

Changes of this entry do not show the "*" in the title.

Description

This number contains the position and the state of the window (maximized) and other flags.

Saved

Only with Appearance set in the File > Configuration > Save Configuration dialog box.