Check if in the default.env file the path to the source file is set in the environment variable GENPATH: #include "File" Path. In addition, you can use the -I: Include File Path compiler option to specify the include file path. With the CodeWarrior IDE, check the access path in the preference panel.