The Compiler Reports an Error, but WinEdit Does not Display it.

This means that WinEdit did not find the EDOUT file, i.e., the compiler wrote it to a place not expected by WinEdit. This can have several causes. Check that the DEFAULTDIR: Default Current Directory environment variable is not set and that the project directory is set correctly. Also in WinEdit 2.1, make sure that the OUTPUT entry in the file WINEDIT.INI is empty.