This is a File I/O function. It is not implemented in the Compiler.
#include <stdio.h>
void setvbuf(FILE *f,
char *buf,
int mode,
size_t size);
setvbuf() is used to specify how a file is buffered. mode determines how the file is buffered.
| Mode | Buffering |
|---|---|
| _IOFBF | Fully buffered |
| _IOLBF | Line buffered |
| _IONBF | Unbuffered |
To make a file unbuffered, call setvbuf() with mode _IONBF; the other arguments ( buf and size) are ignored.
In all other modes, the file uses buffer buf of size size. If buf is NULL, the function allocates a buffer of size size itself.
fflush() and