fmod() and fmodf()

Syntax
  #include <math.h>

  
  double fmod (double x, double y);

  
  float  fmodf(float x, float y);

  
Description

fmod() calculates the floating point remainder of x/y.

Return

The floating point remainder of x/y, with the same sign as x. If y is 0, it returns 0 and sets errno to EDOM.

See also

div(),

ldiv(),

ldexp() and ldexpf(), and

modf() and modff()