Memory Block Functions

Closely related to the string handling functions are those operating on memory blocks. The main difference to the string functions is that they operate on any block of memory, whether it is null-terminated or not. The length of the block must be given as an additional parameter. Also, these functions work with void pointers instead of char pointers.

Listing: ANSI-C Memory Block functions


void * memcpy(void *to, const void *from, size_t size);
void * memmove(void *to, const void *from, size_t size);

int    memcmp(const void *p, const void *q, size_t size);

void * memchr(const void *adr, int byte, size_t size);

void * memset(void *adr, int byte, size_t size);