The ANSI library contains a variety of floating point functions. The standard interface, which is defined for type double, has been augmented by an alternate interface (and implementation) using type float.
double acos(double x); double asin(double x); double atan(double x); double atan2(double x, double y); double ceil(double x); double cos(double x); double cosh(double x); double exp(double x); double fabs(double x); double floor(double x); double fmod(double x, double y); double frexp(double x, int *exp); double ldexp(double x, int exp); double log(double x); double log10(double x); double modf(double x, double *ip); double pow(double x, double y); double sin(double x); double sinh(double x); double sqrt(double x); double tan(double x); double tanh(double x);
The functions using the float type have the same names with an f appended.
float acosf(float x); float asinf(float x); float atanf(float x); float atan2f(float x, float y); float ceilf(float x); float cosf(float x); float coshf(float x); float expf(float x); float fabsf(float x); float floorf(float x); float fmodf(float x, float y); float frexpf(float x, int *exp); float ldexpf(float x, int exp); float logf(float x); float log10f(float x); float modff(float x, float *ip); float powf(float x, float y); float sinf(float x); float sinhf(float x); float sqrtf(float x); float tanf(float x); float tanhf(float x);
In addition, the ANSI library also defines a couple of functions operating on integral values:
int abs(int i); div_t div(int a, int b); long labs(long l); ldiv_t ldiv(long a, long b);
Furthermore, the ANSI-C library contains a simple pseudo-random number generator and a function for generating a seed to start the random-number generator:
int rand(void); void srand(unsigned int seed);