High-Level Inline Assembler for the Freescale RS08

The HLI (High Level Inline) Assembler provides a means to make full use of the properties of the target processor within a C program. There is no need to write a separate assembly file, assemble it and later bind it with the rest of the application written in ANSI-C/C++ with the inline assembler. The Compiler does all that work for you. For more information, refer to the RS08 Reference Manual.