There is a language extension in the Compiler for ANSI-C. You can use keywords to qualify pointers in order to distinguish them, or to mark interrupt routines.
The Compiler supports the following non-ANSI compliant keywords (see Backend if they are supported and for their semantics):