Guidelines

The -La option translates specified parts of header files into an include file to import labels and defines into an assembler source. Because the -La compiler option is very powerful, its incorrect use must be avoided using the following guidelines implemented in a real project. This section describes how the programmer uses this option to combine C and assembler sources, both using common header files.

The following general implementation recommendations help to avoid problems when writing software using the common header file technique.