The Compiler Frontend reads the source files, does all the syntactic and semantic checking, and produces intermediate representation of the program which then is passed on to the Backend to generate code.
This chapter discusses features, restrictions, and further properties of the ANSI-C Compiler Frontend.