Product Defines

The following table shows the Defines identifying the Compiler. The Compiler is a HI-CROSS+ Compiler (V5.0.x).

Table 1. Compiler Identification Defines
Name Defined
__PRODUCT_HICROSS_PLUS__ defined for V5.0 Compilers
__DEMO_MODE__ defined if the Compiler is running in demo mode
__VERSION__ defined and contains the version number, e.g., it is set to 5013 for a Compiler V5.0.13, or set to 3140 for a Compiler V3.1.40