Option Groups

Compiler options are grouped by:

A special group is the STARTUP group: The options in this group cannot be specified interactively; they can only be specified on the command line to start the tool.

Refer to the following table:

Table 1. Compiler Option Groups
Group Description
HOST Lists options related to the host
LANGUAGE Lists options related to the programming language (e.g., ANSI-C)
OPTIMIZATIONS Lists optimization options
OUTPUT Lists output file generation options (types of file generated)
INPUT Lists options related to the input file
CODE GENERATION Lists options related to code generation (memory models, float format, etc.)
MESSAGES Lists options controlling error message generation
VARIOUS Lists various options
STARTUP Options specified only on tool startup

The group corresponds to the property sheets of the graphical option settings.

Note: Not all command line options are accessible through the property sheets as they have a special graphical setting (e.g., the option to set the type sizes).