Option Detail Description

The remainder of this section describes each of the Compiler options available for the Compiler. The options are listed in alphabetical order. Each is divided into several sections listed in the following table.

Table 1. Compiler Option - Documentation Topics
Topic Description
Group HOST, LANGUAGE, OPTIMIZATIONS, OUTPUT, INPUT, CODE GENERATION, MESSAGES, or VARIOUS.
Scope Application, Compilation Unit, Function, or None
Syntax Specifies the syntax of the option in an EBNF format
Arguments Describes and lists optional and required arguments for the option
Default Shows the default setting for the option
Defines List of defines related to the compiler option
Pragma List of pragmas related to the compiler option
Description Provides a detailed description of the option and how to use it
Example Gives an example of usage, and effects of the option where possible. compiler settings, source code and Linker PRM files are displayed where applicable. The example shows an entry in the default.env for a PC.
See also Names related options