After successful compilation, the Compiler generates an object file containing the target code as well as some debugging information. This file is written to the directory listed in the OBJPATH: Object File Path environment variable. If that variable contains more than one path, the object file is written in the first listed directory. If this variable is not set, the object file is written in the directory the source file was found. Object files always get the extension *.o.