Environment Variable Details

The remainder of this chapter describes each of the possible environment variables. The following table lists these description topics in their order of appearance for each environment variable.

Table 1. Environment Variables - Documentation Topics
Topic Description
Tools Lists tools that use this variable.
Synonym A synonym exists for some environment variables. Those synonyms may be used for older releases of the Compiler and will be removed in the future. A synonym has lower precedence than the environment variable.
Syntax Specifies the syntax of the option in an EBNF format.
Arguments Describes and lists optional and required arguments for the variable.
Default Shows the default setting for the variable or none.
Description Provides a detailed description of the option and how to use it.
Example Gives an example of usage, and the effects of the variable where possible. The example shows an entry in the default.env for a PC.
See also Names related sections.