View Menu

The View menu enables you to customize the application window. You can define things such as displaying or hiding the status or toolbar. You can also define the font used in the window, or clear the window. The following image shows the View Menu options.

Figure 1. View Menu
View Menu

The following table lists the View Menu options.

Table 1. View Menu Options
Menu Option Description
Toolbar Switches display from the toolbar in the application window.
Status Bar Switches display from the status bar in the application window.
Log Allows you to customize the output in the application window content area. The following entries are available when Log is selected:
Change Font Opens a standard font selection box. The options selected in the font dialog box are applied to the application window content area.
Clear Log Allows you to clear the application window content area.