A filename is dragged from an external application (for example the File Manager/Explorer) and dropped into the Compiler window. The dropped file is compiled as soon as the mouse button is released in the Compiler window. If a file being dragged has the *.ini extension, it is considered to be a configuration and it is immediately loaded and not compiled. To compile a C file with the *.ini extension, use one of the other methods.