Use the Save Configuration dialog box to configure which parts of your configuration you want to save to the project file.
The Save Configuration dialog box offers the following options:
Check this option to save the current option and message settings when a configuration is written. By disabling this option, the last saved content remains valid.
Check this option to save the current editor setting when a configuration is written. By disabling this option, the last saved content remains valid.
Check this option to save items such as the window position (only loaded at startup time) and the command line content and history. By disabling this option, the last-saved content remains valid.
Check this option to save the environment variable changes made in the Environment configuration dialog box.
The application writes the configuration on exit. No question dialog box appears to confirm this operation. If this option is not set, the application will not write the configuration at exit, even if options or another part of the configuration have changed. No confirmation appears in either case when closing the application.