Option Settings Dialog Box

The Option Settings dialog box enables you to set or reset application options. The possible command line option is also displayed in the lower display area The available options are arranged into different groups. A sheet is available for each of these groups. The content of the list box depends on the selected sheet (not all groups may be available). The following table lists the Option Settings dialog box selections.

Figure 1. Option Settings Dialog Box
Option Settings Dialog Box
Table 1. Option Settings Dialog Box Tabs
Tab Description
Optimizations Lists optimization options.
Output Lists options related to the output files generation (which kind of file to generate).
Input Lists options related to the input file.
Language Lists options related to the programming language (ANSI-C)
Target Lists options related to the target processor.
Host Lists options related to the host operating system.
Code Generation Lists options related to code generation (such as memory models or float format).
Messages Lists options controlling the generation of error messages.
Various Lists options not related to the above options.

Checking the application option checkbox sets the option. To obtain more detailed information about a specific option, click once on the option text to select the option and press the F1 key or click Help .

Note: When options requiring additional parameters are selected, you can open an edit box or an additional sub window where the additional parameter is set. For example, for the option Write statistic output to file available in the Output sheet.