Help Menu

The Help Menu enables you to either display or hide the Tip of the Day dialog box at application startup. In addition, it provides a standard Windows Help entry and an entry to an About box. The following image shows the Help Menu.

Figure 1. Help Menu
Help Menu

The following table lists the Help Menu options.

Table 1. Help Menu Options
Menu Option Description
Tip of the Day Switches on or off the display of a Tip of the Day during startup.
Help Topics Standard Help topics.
About Displays an About box with some version and license information.