Enter the Service Name , Topic Name , and the Client Command for the DDE connection to the editor (Microsoft Developer Studio [Editor Started with DDE (Microsoft Developer Studio)] or UltraEdit-32 [Editor Started with DDE (UltraEdit-32)]). The Topic Name and Client Command entries can have modifiers for the filename, line number, and column number as explained in Modifiers.
For Microsoft Developer Studio, use the settings in the following listing.
Service Name : msdev Topic Name : system Client Command : [open(%f)]
UltraEdit-32 is a powerful shareware editor. It is available from www.idmcomp.comwww.idmcomp.comwww.idmcomp.com or www.ultraedit.com, email idm@idmcomp.com. For UltraEdit, use the following settings.
Service Name : UEDIT32 Topic Name : system Client Command : [open("%f/%l/%c")]