The content area displays the logging information about the compilation process. This logging information consists of:
When you drag and drop a file into the Compiler window content area, the Compiler either loads it as a configuration file or compiles the file. It loads the file as configuration file, if the file has the *.ini extension. Otherwise, the compiler processes the file using the current option settings.
All of the text in the Compiler window content area can have context information consisting of two items:
File context information is available for all source and include files, for output messages that concern a specific file, and for all output that is directed to a text file. If a file context is available, double-clicking on the text or message opens this file in an editor, as specified in the Editor Configuration. Also, a right-click in this area opens a context menu. The context menu contains an Open entry if a file context is available. If a context menu entry is present but the file cannot be opened, refer to the Global Initialization File (mcutools.ini).
The message number is available for any message output. There are three ways to open the corresponding entry in the help file.
If the selected line does not have a message number, the main help displays.
If the selected line does not have a message number, the main help displays.
This entry is available only if a message number is available in the RS08 Compiler Message Settings Dialog Box .