You can use the RS08 compiler as a standalone compiler. This tutorial does not create an entire project with the Build Tools, but instead uses parts of a project already created by the CodeWarrior
New Bareboard Project wizard.
Note:
Although it is possible to create and configure a project from scratch using the standalone Build Tools, it is easier and faster to create, configure, and manage your project using the CodeWarrior Projects wizard.