RS08 Compiler > Type Sizes

Use this panel to specify the available data type size options for the RS08 Compiler.

The following figure shows the Type Sizes panel.

Figure 1. Tool Settings - RS08 Compiler > Type Sizes
Tool Settings - RS08 Compiler > Type Sizes
Note: For information about the description of the options available in the Type Sizes panel for RS08 compiler, refer to the -T: Flexible Type Management topic.