RS08 Compiler > Optimization > Optimize Library Function

Use this panel to configure the optimize library function options for the RS08 compiler.

The following figure shows the Optimize Library Function settings.

Figure 1. Tool Settings - RS08 Compiler > Optimization > Optimize Library Function
Tool Settings - RS08 Compiler > Optimization > Optimize Library Function
Note: For information about the description of the options available for the OptimizeLibrary Function panel for RS08 compiler, refer to the -OiLib: Optimize Library Functions topic.