Use this panel to specify other flags for the RS08 Compiler to use.
The following figure shows the General panel.
The following table lists and describes the General options for RS08 compiler.
| Option | Description |
|---|---|
| Other flags | Specify additional command line options for the compiler; type in custom flags that are not otherwise available in the UI. |