RS08 Compiler Build Settings Panels

The following sections describe the settings panels that configure the RS08 Compiler build properties. These panels are part of the project's build properties settings, which are managed in the Properties window. To access these panels, proceed as follows:

  1. Select the project for which you want to set the build properties, in the CodeWarrior Projects view.
  2. Select Project > Properties from the IDE menu bar.

    The Properties for < project > dialog box appears.

  3. Expand the C/C++ Build tree control and select Settings.

The various settings for the build tools are displayed in the right panel. If not, click on the Tool Settings tab.

The options are grouped by tool, such as Messages , Host , General , Disassembler, Linker, Burner, HCS08Compiler, HCS08 Assembler, and Preprocessor options.

Depending on the build properties you wish to configure, select the appropriate option in the Tool Settings tab page.

Note: For information about other build properties panels, refer to the Microcontrollers V10.x Targeting Manual.

The following table lists the build properties panels for the RS08 Compiler.