Use this panel to specify the command, options, and expert settings for the build tool compiler. Additionally, the RS08 Compiler tree control includes the general, include file search path settings.
The following figure shows the RS08 Compiler settings.
The following table lists and describes the compiler options for RS08.
| Option | Description |
|---|---|
| Command | Shows the location of the compiler executable file. Default value is : " ${HC08Tools}/crs08.exe". You can specify additional command line options for the compiler; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the compiler will be called with. |
| Expert Settings | Shows the expert settings command line parameters; default is {COMMAND} ${FLAGS}${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}. |
| Command line pattern |