It allows you to view and edit the properties of a component.
To add the properties of a component, right-click the Properties element and select Add Property option from the context menu. To select the type of property, select Property Type from the drop-down list. Each Property Type dynamically modifies the editor showing only the features for that particular property.
The panel on the left contains the list of the properties, and the features of the currently selected property are displayed on the right side. These features influence the behavior of the property in Processor Expert environment.
The properties can be reordered and copied using context menu as shown in figure below.