Driver editor

It allows you to edit component driver file.

Driver built-in editor serves for editing implementation of methods and events, and includes HTML help files and other files generated by the CDE. The component driver can be edited by selecting the driver file, select Drivers > sw ><name of the component>.drv file as shown in the figure below.

Figure 1. Component driver file



The driver editor supports all features supported by the Eclipse Editor. The following are Processor Expert features:

The following figures show all the above features.

Figure 2. Driver editor



Figure 3. Driver editor