Component editor

It holds the high level information related to the component, such as author version, the icon to show the copyright information when loaded in Processor Expert.

In the Component Editor, the project name is different from the component name. Every component is represented as a tree of elements, such as Methods, Properties, and Events. Each element has a context menu and an associated editor. The Component Editor is divided into two panels.
Figure 1. Component editor screen



This table explain the fields of Component Editor.

Table 1. Component details
Field Description
Header  
Name Name of the component
Description Short description of the component
Author Author's name, that will appear in the source code header
Version Version number of the component. To indicate a beta version, use format 00.9XX. When you save the CDE, it will ask you if a new revision needs to be added
Icon Component icon name, relative path to .bean without extension
Types File Comma-separated list of types-files (*.tps), relative path from Beans\, without extension
File Version Component file format
Options Contains component specific options (CDE UI provides tool tip with detailed description)
Help Contains configuration of help style
Help type Define list of preselected help pages (templates)
Help Files List of help files with proper order based on selected type
Auto Save Driver Driver is saved automatically
Detailed Help Displays the detailed help
Auto Save Help Auto saves the help
Compiler Select the compiler that can be used