Every property defines the unique symbol in the component. The symbol is the name of the macro defined for the component driver in the Processor Expert.
The symbol should not begin with the character underscore '_'. The value of the macro is value of the property set in Processor Expert Component Inspector.
Some properties have detailed information defined as macros. The name of the macro is completed from the name of the property (feature Symbol) and the suffix. The suffix depends on the type of the property. The following properties have defined the detailed information:
Macro without suffix - the list of lines of the text. If user does not enter any text, the macro is not defined.