Macroprocessor command starts with character % as first non-space character on line and then follows command-identifier and parameters. The rest of line is ignored and can be used as a comment.
Here is complete description of commands supported in basic version of CDE. Commands are divided into several groups according to its function.