A macro definition is one or more assembly statements that define:
To define a macro, use the .macro directive.
The .macro directive is part of the first line of a macro definition. Every macro definition ends with the .endm directive .The following listing and table shows the full syntax, and explains the syntax elements, respectively.
name: .macro [ parameter ] [ ,parameter ] ... macro_body .endm
| Element | Description |
|---|---|
| name | Label that invokes the macro. |
| parameter | Operand the assembler passes to the macro for us in the macro body. |
| macro_body | One or more assembly language statements. Invoking the macro tell the assembler to substitutes these statements. |
The body of a simple macro consists of just one or two statements for the assembler to execute. Then, in response to the .endm directive, the assembler resumes program execution at the statement immediately after the macro call.
But not all macros are so simple. For example, a macro can contain a conditional assembly block, The conditional test could lead to the .mexit directive stopping execution early, before it reaches the .endm directive.
The following listing is the definition of macro addto, which includes an .mexit directive.
//define a macro addto .macro dest,val .if val==0 no-op .mexit // execution goes to the statement // immediately after the .endm directive .elseif val==1 // use compact instruction add #1, dest .mexit // execution goes to the statement // immediately after the .endm directive .endif // if val is not equal to either 0 or 1, // add dest and val add val, dest // end macro definition .endm
The following listing shows the assembly-language code that calls the addto macro.
// specify an executable code section .text xor d0,d0 // call the addto macro addto d0,0 addto d0,1 addto d0,2 addto d0,3
The following listing shows the expanded addto macro calls.
xor d0,d0 nop add d0 add d0,2 add d0,3