Tells the assembler to take input from the specified file.
.include filename
filename
Name of an input file.
When the assembler reaches the end of the specified file, it takes input from the assembly statement line that follows the .include directive. The specified file can itself contain an .include directive that specifies yet another input file.