MQXLite_task components are dynamically created when changing the Task Template List property of the MQX Lite component. Based on the defined number of application tasks, the corresponding number of MQXLite_task components are created and assigned as inherited components (see chapter "Component Inheritance and Component Sharing" of the Processor Expert User Guide). Use the options in the Component Inspector of the particular MQXLite_task to set up the tasks.