The Processor Expert technology also enables adding MQX Lite RTOS to existing applications. The following steps describe how to add MQX Lite RTOS to an existing application.
Configure the MQX Lite operating system and define number of application tasks according to the application needs. For more information, refer to the MQX Lite Component Interface and MQXLite_task Component Interface sections.