About the product

The S32R264 Development Package is an optional software package that can be installed on S32DS for Power Architecture in order to provide support for the S32R26x family of processors. The development package cannot be run as a standalone application, nor can it be integrated with third-party software products.

S32DS for Power Architecture with the installed S32R264 Development Package features the following options: