Trace Commander view is used to manage the trace collection data. The view is used to perform actions such as, start, stop trace on different trace generators, manual upload or trace configuration for data trace collection.
Trace Commander is based on an xml platform configuration file, which is responsible for configuring all the modules included in the target architecture. Hence, the Trace Commander tool is used to ease the task of configuring and uploading trace.
Trace Commander displays all the modules from a platform configuration file. Perform the following steps in order to collect multi core trace data using Trace Commander:
The Trace Commander view is displayed.

The Trace Commander view displays all trace generators and trace buffers available in the selected platform file. The colors suggest if they are available or not for collecting trace. Green means the trace generator is enabled and grey means that the trace generator is disabled.


to
Connect.When the session is started the button looks like this
, meaning the target is configured using the
selected platform file. This will be attached to the active debug session. The
configuration is applied on the whole platform. Now the trace buffer and trace
generators selection and configuration becomes unavailable.

Trace data is saved in .AnalysisData folder from the application’s workspace.

Export
: exports the current displayed configuration
file.