On the main menu, click Help > Installation Details.
In the S32 Design Studio for S32 Platform Update 2 Installation Details dialog
box, open the Installed Software tab. Select the software
to be removed and click Uninstall.
In the message box, click Yes to confirm the review of
components to be uninstalled from S32 Design Studio for S32 Platform Update 2. Click
Finish to complete the operation.
When the uninstall operation is done, restart S32 Design Studio for S32 Platform Update 2.