S32 Design Studio for S32 Platform Update 2 provides a tool to help you find and install the latest
product updates and additional software packages. The lookup is performed across the sites
that are specified in the user preferences.
To preview and edit the list of software sites, click on the menu. In the Preferences dialog box, click
Install/Update and Available Software Sites.
The right pane displays the list of software sites that are scanned for available updates
automatically. You can manage the software sites using the buttons located at the right border
of the dialog box:
- Add: Click to add a new site. Specify a custom name of the site
and the location - a URL, a local directory, or a locally stored archive file.
- Edit: Click to modify the name and location of the selected site.
To select a site, click it in the list. The selected site is highlighted.
- Remove: Click to remove the selected site from the list.
- Reload: Click to load the information about available updates
from the selected site.
- Enable/Disable: Click to flag the selected
site, or to remove the flag from the selected site.
- Import: Click to add sites from the specified XML file.
- Export: Click to export flagged sites to an XML file.