Loading an SDK

You can add an external SDK to your workspace using the SDK descriptor provided in the XML format. When added to a workspace, the loaded SDK becomes available for use in all projects with the compatible settings. The SDK source files are not copied to the product or workspace directory.

To load an SDK to your workspace:

  1. Click Window > Preferences on the main menu. Then go to S32 Design Studio for S32 Platform > SDK Management.
  2. Click the Load... button.
  3. Browse to the folder where the SDK is located and select the XML descriptor.
  4. Click Open to confirm the loading.
    Once done, the loaded SDK appears on the SDK Management page.
If there are some changes in original SDK after the loading, you can click the Reload button to be in sync with the latest updates. Alternatively, click Remove and use the Load button to add the updated version.