The following table describes the settings that you can configure on this page.
| Option | Description |
|---|---|
| Project Name | The name assigned to the project on the General
properties wizard page. Note: This name cannot be edited in-place.
Click Back to specify a different name on the
General properties page.
|
| Core |
The ArmĀ® core used in the selected processor. Note: This check box cannot be cleared. Click Back to
select a different processor on the General properties
page.
|
|
FPU Support |
This setting enables GCC to build a project with the floating point support provided either by the processor or by a software library. The availability of options depends on the ArmĀ® core and ToolChain selection. Options:
Note: Find more information about Arm options in the GCC toolchain documentation on
the web.
|
|
Language |
This setting sets up the default compiler, linker, and preprocessor options for the toolchain and configures other project files, such as main, for the target language. Note: The selected programming language defines the toolchain settings for the
linker and compiler that will be available in the properties for the created
project. Selecting C limits the toolchain options to this
specific language. If you select C++, you will be able to
configure settings for the C and C++ compiler, linker, and preprocessor. The
toolchain settings can be further configured after creating the project. For
details, see section "C/C++ Build Tool Settings".
Options:
|
|
SDKs |
This setting allows you to select an SDK to be added to the project. Click the search button
(...) to select an SDK from the list.
Default: SDK is not
selected.Note: The
Select SDK window lists the SDKs available in S32 Design Studio for S32 Platform Update 2. If you do not see your SDK, add it on the SDK Management page. Find the details in Adding an SDK.
|