Applying the license during installation

To apply the license when installing S32 Design Studio for S32 Platform Update 2:

  1. Get the activation code as described in topic Obtaining the activation code.
  2. When requested, enter the activation code and click OK.


    Enter the activation code

    If you click Cancel, the installation rolls back.

  3. After the code is entered, choose the activation type. Click Online for the installer to complete the activation without your interference.


    Select the activation type

    Click Offline to submit the activation files manually. This option may be useful if you are not connected to the Internet.

  4. If you click Offline, the installer generates the activation request. Perform the following steps:
    1. Save the request.xml file in a local folder.
    2. Browse to www.nxp.com and log in with your registered member credentials.
    3. On the web page, go to Offline Activation. Browse to the request.xml file that you saved recently and click Process. Then save the generated activation.xml file in a local folder.


      Select the activation type

    4. Get back to the installer. In the Activation response dialog box, browse to the activation.xml file and click Load.
Once done, the activation step is passed and the installation continues.