| Hardware |
Specify the settings related to the target:
- Select device and core: Click
this button and pick the target processor and the
core from the list. The data appears in the
Device and
Core fields.
- Initialization script: The
path of the generic initialization script generated
automatically.
To specify the
script particular to your evaluation board, go to
the following folder:
<S32 Design Studio for S32 Platform Update 2 installation
folder>/S32DS/tools/S32Debugger/Debugger/scripts/s32xxxx
The
last folder in the path is named as your target
processor, for instance,
/s32v234. Find the
information about the available script files in
the readme file located in
this folder.
- Initial core: Enable this
option if the debug configuration will start the
first debug session in a launch group or the only
debug session in single-core debugging. When
enabled, this option indicates that the evaluation
board needs to be initialized.
In multi-core
debugging, make sure to disable this option in all
debug configurations that start the second and all
later debug sessions in a launch group.
Note: When disabled, the Initial
core option makes the probe connection
settings, JTAG settings, and GDB server settings
(below) unavailable.
|
| Debug Probe Connection |
Configure the connection between the board and the
computer.
- Interface: Specify the
connection interface.
- USB device: For the USB
connection, specify the COM port to which the board
is connected.
If the board is not connected with
the USB cable, connect it and wait for the probe's
TX/RX indicator to get green. Then click
Refresh for the connected
COM port to appear on the
Port menu.
If you
have a problem with the USB connection:
- On Windows, install the S32 Debug Probe driver
manually. For details, refer to readme.txt in
S32DS/tools/S32Debugger/Debugger/drivers/usb/.
- On Linux, install the udevadm utility,
this tool detects the used port.
- Hostname or IP: For the
Ethernet connection, specify the host name or IP
address of the probe network adapter.
Note: To learn
the host name of the probe, refer to the
documentation provided with the delivery kit. For
the static IP address assigned to the probe,
consult your network administrator.
- Test connection: click the
button to check the connection.
|
| JTAG Communication Speed |
Specify the JTAG communication settings.
- JTAG Speed (KHz): Specify the
JTAG speed.
- Timeout: Specify the JTAG
timeout.
- Delay after reset: Enable
this option to perform software reset on the device
at the beginning of the debug session. Specify the
board initialization delay (in milliseconds).
|
| GDB server |
Specify the GDB server settings.
|
| GDB Client |
Specify the GDB client settings:
- Executable: The path of the
GDB client. This path is generated automatically
when you click the Select device and
core button and select the target
device and the core.
- Commands: If required,
specify commands to be executed after the GDB client
is started. These commands are executed next to the
commands specified on the
Startup tab.
- Force thread list update on
suspend: Enable this option for the
thread list to be updated forcedly if the debug
session is suspended.
|
| Semihosting |
Configure semihosting, that is, the ability of the debug
session to send output to the Console
view.
- Enable semihosting: Enable
semihosting.
- Port: The port for
semihosting. Read-only. The port number is defined
as (GDB server port +1). Default: 45001.
Note: If semihosting is enabled, the semihosting
console needs to be opened in the
Console view once the debug
session is started.
|
| Secure debugging |
Configure settings for secured chips.
- Enable secure debugging: Enable this option
to start a debug session on locked chip.
- Debugging type: Select the authentication
method. Options: Password, Challenge &
Response.
- Clear data stored: Click the
button to delete any data from secure storage.
Note: The availability and support of the option
depends on the target device.
Note: If the chip is unlocked, enabling secure debuging is
meaningless.
|