Debugging with S32 Debug Probe

The following topics describe how to debug a bare-metal application on the board connected to the computer with the S32 Debug Probe:
Note: Running of an S32 Debugger session may sometimes end with errors of GDB version determining. In some machines the GDB version request can be proceeded longer than expected. To solve this problem, go to Window > Preferences > S32 Design Studio for S32 Platform Update 2 > S32 Debugger. In the GDB version request maximum delay (sec) field increase the value in the 5-seconds step. Click Apply and Close. Then try to run the debug session again.