|
|||||||||
| PREV CLASS NEXT CLASS | FRAMES NO FRAMES | ||||||||
| SUMMARY: NESTED | ENUM CONSTANTS | FIELD | METHOD | DETAIL: ENUM CONSTANTS | FIELD | METHOD | ||||||||
java.lang.Objectjava.lang.Enum<Mode>
org.simpleframework.xml.stream.Mode
public enum Mode
The Mode enumeration is used to specify the output
mode for XML text. This is used by the OutputNode
to describe if element text will be escaped or wrapped in a
CDATA block. The mode is a three state object, the third of the
states indicates whether an explicit state has been set or not.
If a specific state has not been set then the node will inherit
its output mode from the last parent to have it set.
OutputNode| Enum Constant Summary | |
|---|---|
DATA
Indicates that data written will be within a CDATA block. |
|
ESCAPE
Indicates that data written will be escaped if required. |
|
INHERIT
Indicates that the mode will be inherited from its parent. |
|
| Method Summary | |
|---|---|
static Mode |
valueOf(java.lang.String name)
Returns the enum constant of this type with the specified name. |
static Mode[] |
values()
Returns an array containing the constants of this enum type, in the order they are declared. |
| Methods inherited from class java.lang.Enum |
|---|
clone, compareTo, equals, finalize, getDeclaringClass, hashCode, name, ordinal, toString, valueOf |
| Methods inherited from class java.lang.Object |
|---|
getClass, notify, notifyAll, wait, wait, wait |
| Enum Constant Detail |
|---|
public static final Mode DATA
public static final Mode ESCAPE
public static final Mode INHERIT
| Method Detail |
|---|
public static Mode[] values()
for (Mode c : Mode.values()) System.out.println(c);
public static Mode valueOf(java.lang.String name)
name - the name of the enum constant to be returned.
java.lang.IllegalArgumentException - if this enum type has no constant
with the specified name
java.lang.NullPointerException - if the argument is null
|
|||||||||
| PREV CLASS NEXT CLASS | FRAMES NO FRAMES | ||||||||
| SUMMARY: NESTED | ENUM CONSTANTS | FIELD | METHOD | DETAIL: ENUM CONSTANTS | FIELD | METHOD | ||||||||