Beginning with peripheral selection
You can select the peripheral in the Routing Details view and the
Peripheral Signals view.
- Select the Peripheral.
- In Routing Details view, select one of the available Signals or expand the peripheral in Peripheral Signals view.
- Selected the desired pin/internal signal. Items (pins/internal signals) in the Routed pin/signal column in the Routing Details view have following decorators:
- Exclamation mark and default text color indicates that such item selection causes a register conflict or the item cannot be routed to the selected peripheral signal (some other peripheral signal can be).
- Exclamation mark and gray text color indicates that the
item cannot be routed to any signal of the selected peripheral. The
item is available for different peripheral using the same signal.
Note: Route to field in Routing details view contains items that are connectable to the selected signal (without its channel if applicable). So when selected signal is “GPIO, 6” then the Routed pin/signal provides items connectable to “GPIO”.
Figure 1. Defining routing path