DCF Problems View

Problems view will indicate if the DCF tool has a problem.

The tool will perform the following verifications:

  • DCF Image oversize. If at any point, import of MEX configuration, DCF binary, or current modification, the image gets above 5368 bytes, the tool will automatically generate an error.
  • Empty Data Word, Control Word or Address textfields.
  • Invalid value in Data Word, Control Word, Chip Select, Address, Target Module and Client Selection. Either the input has no recognized number format, or the value is too big.
  • The Control Word value does not set the last bit to 1.
  • The value written in the Data Word field does not fit in the current available bitfields (when a Target Module and Client Selection is selected).
Figure 1. Problems View